AXIS#.ICONT
Description
AXIS#.ICONT returns the drive continuous rated current in Arms.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
Arms |
Range |
N/A |
Default Value |
N/A |
Data Type |
Float |
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
AXIS1.ICONT |
5000h |
0bh |
Signed32 |
- |
1000:1 |
Read only |
No |
AXIS2.ICONT |
5100h |
0bh |
Signed32 |
- |
1000:1 |
Read only |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.ICONT |
5013 |
1395 |
Signed32 |
Read Only |
- |
AXIS2.ICONT |
70549 |
1139 |
Signed32 |
Read Only |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.ICONT |
5013 |
Float |
Read Only |
- |